6/22/2011 12:11 PM | |
Posts: 47 Rating:
|
Dear All Can any one share me a document expalination clearly that When and why we use control mode as bellow (I mention in Simovert Master Drive). 0: v/f contol with superposed speed control (only for P095 = 2, 10, 11) 1: v/f control (only for P095 = 2, 10, 11, 13) 2: v/f control for textile applications; allows no frequency corrections (e.g. by the current limitation controller) (only for P095 = 2, 10, 11) 3: Frequency control (without tachometer) (only for P095 = 2, 10, 11, 13) 4: Speed control (only for P095 = 2, 10, 11, 12) 5: Torque control (only for P095 = 2, 10, 11, 12) In function diagram: 14 and 420 |
6/22/2011 5:48 PM | |
Joined: 7/8/2009 Last visit: 7/26/2023 Posts: 1974 Rating:
|
Its bit difficult to find Documents for Explanation but you can try customer by explaning him Basics about All modes.. There is very good Explanation in Following Manual Operating Instructions: MICROMASTER 440 0,12 kW - 250 kW Please Refer Page 235 onwards Regards Devesh Vithani |
I dont Like people driving Fast, thats the reason I overtake them ;) |
|
Follow us on