11/2/2023 5:55 AM | |
Joined: 3/14/2008 Last visit: 8/13/2024 Posts: 2084 Rating:
|
Hi, There is an easier option, if you want to change I/O that is not visible in the POV view, you can do as follows: 1. Right click on a field in the PO view and select: Process Objects->Select I/Os 2. Go to filter by column and under I/O name enter the I/O name you want to have in the PO view 3. Click on OK 4. When the search is completed, select all I/O and select the "Parameters" column and click on OK Now, all I/O is available in the PO view. You can change the values and normally after I'm done I repeat the process and deselect all I/O which was set as parameter to keep the project clean. |
If I could help you, you can use the RATE button. Thank you. |
|
Follow us on