10/5/2005 4:04 PM | |
Joined: 9/29/2005 Last visit: 2/24/2025 Posts: 25 Rating:
|
Hello I have a problem with setting the date and time in a TP170B. I use WinCC Flexible 2005. I have done this before but with protool with out any problems. Now I set up a area poiter for "this connection" in WinnCC Flexible 2005, but It will not adjust the date and time in the windows CE. I have to do that manually. Is it wrong setting it up this way? and do I need to do something else to make it work. I had the same problem with WinCC Flexible 2004, so It has nothing to do with that, I must do something wrong. If someone have experience with this please let me know Brg. Morten |
10/13/2005 1:09 PM | |
Posts: 10 Rating:
|
Hello You can look and the following links for more information to WinCC flexible and the area pointer date and time. http://support.automation.siemens.com/WW/view/en/19355865 http://support.automation.siemens.com/WW/view/en/19353440 |
Follow us on