8/6/2024 9:44 AM | |
Joined: 3/11/2019 Last visit: 11/6/2024 Posts: 1653 Rating: (303)
|
Hi, check this setting mentioned for monitoring of SCL blocks in TIA. Program status display for SCL programsIf no values can be displayed for a tag, the corresponding cell has a yellow background and three question marks are shown. In this case, select the "Create extended status information" check box in the properties of the block and download the block to the device again. All values are then displayed. regards sancruz |
Feedback appreciated, please rate |
|
8/6/2024 1:14 PM | |
Joined: 3/30/2020 Last visit: 11/6/2024 Posts: 4930 Rating: (1008)
|
I can see that the assignment is not pushed through to the array entry. Have you tried going through a temporary memory bit first -- just as a test. Did you patch your software yet? Perhaps it will be a good idea to contact Siemens and show them what you have there. Have a look at this topic: SCL program is not executed correctly after compiling in TIA Portal ! |
Activities of this user is voluntary. There is no obligation or liability placed on this user. Though optional, your 'please' and 'thank you' is highly valued. |
|
Follow us on