11/22/2012 9:48 AM | |
Joined: 8/31/2010 Last visit: 1/9/2025 Posts: 1523 Rating: (230) |
Hello GOWDA, Arrays are not possible in WinCC Professional v11 as it is the similar case in WinCC v7.0 Whereas you have the option of creating Arrays in WinCC Advanced v11. Have a look @ Working with Tags |
Like it? Rate it! |
|
11/22/2012 10:03 AM | |
Posts: 112 Rating: (2) |
dear Ganes I Have gon through it ........ but is there any other way to simeler as an array or to readuce the tag limit in WinCC Professional v11.0.............. |
11/22/2012 11:06 AM | |
Joined: 8/31/2010 Last visit: 1/9/2025 Posts: 1523 Rating: (230) |
Hello GOWDA, May be you can make use of the below system functions in WinCC Professional v11 SetBitInTag ResetBitInTag InvertBitInTag wherein you can define one DWORD instead of 32 BOOL and make use of it in your screens. This is one way of doing. |
Like it? Rate it! |
|
11/22/2012 11:25 AM | |
Posts: 112 Rating: (2) |
dear Ganes I Have gon through it ........ but is there any other way to simeler as an array or to readuce the tag limit in WinCC Professional v11.0.............. Hello GOWDA, May be you can make use of the below system functions in WinCC Professional v11 SetBitInTag ResetBitInTag InvertBitInTag wherein you can define one DWORD instead of 32 BOOL and make use of it in your screens. This is one way of doing. dear sir ok sir thanks for kind replay did you know knowlage abt (RAW) DATA TYPE what is an use it.................... |
11/23/2012 12:46 PM | |
Posts: 3037 Rating: (192)
|
Hello GOWDA, |
11/24/2012 2:15 PM | |
Posts: 112 Rating: (2) |
dear all i have gone through the link............................. is there any structrual tagging methord so that i can import the tags of the db directely from PLC like an wincc .............. |
Last edited by: GOWDA at: 11/24/2012 2:16 PM |
|
11/25/2012 11:32 AM | |
Joined: 8/31/2010 Last visit: 1/9/2025 Posts: 1523 Rating: (230) |
Hello Gowda, Do you mean structure tags of WinCC?? If it is so the this is it;s equivalent in TIA Portal. Working with User Data types |
Like it? Rate it! |
|
11/26/2012 4:43 AM | |
Posts: 112 Rating: (2) |
dear all i have gone through the link............................. is there any structrual tagging methord so that i can import the tags of the db directely from PLC like an wincc .............. Hello Gowda, Do you mean structure tags of WinCC?? If it is so the this is it;s equivalent in TIA Portal. Working with User Data types Dear Tweety& ganes, THIS WAT i am searching thanks for kind replay.................. |
Last edited by: GOWDA at: 11/26/2012 4:45 AM |
|
Follow us on