8/23/2024 3:48 PM | |
Joined: 11/21/2020 Last visit: 9/30/2024 Posts: 159 Rating: (0) |
Hi, Frome here I stole an idea of how to use an array of digital alarms: https://www.solisplc.com/tutorials/alarms-and-diagnostics-in-siemens-tia-portal I couldn't digest all it all, because I haven't dealt with state machines untile now, and I really don't need them anyways. What I got at the end of an experiment is in attached pdf (it is very simple), and it is somehow working, but I am not sure is it reccomendable/ligal way to manage alarms. How does it works anyways, Alarm_Inupt_0 - 15 input tags are NO bools, but when I close %M51.1, which is connected to Alarm_Input_0 in "Main" block - alarm is activated? AttachmentBinder1.pdf (75 Downloads) |
Last edited by: milos23 at: 08/23/2024 16:57:29 |
|
Follow us on