1/23/2015 2:01 PM | |
Joined: 6/27/2012 Last visit: 4/22/2025 Posts: 8 Rating:
|
Unfortunately i dont have any answer for this, just another question. We are building an AS-i network(total 150m AS-i cable)with safety components on the bus, at power up andfinishedconfiguration, we discovered telgram problems with 2 slaves of total 31. It is an extendermountedat the end of the line. An repeater and AS-i power supply was mountedapproximately 100meters from the DP/AS-i F-Link. The result was that all slaves after the repeater failed. I have attempted to re-locate the repeater closer and further away from theDP/AS-i F-Link. Have checked polarity, voltage drop, connections and so on... I`m running out of suggestion. Someone with experiences, that can help us further?
----------- New subject after splitting from ASI TROUBLESHOOTING HELP NEEDED. |
Last edited by: Min_Moderator at: 1/23/2015 3:51 PMSplitted |
|
Follow us on