4/1/2017 10:46 AM | |
Joined: 12/22/2006 Last visit: 1/25/2022 Posts: 1742 Rating: (308) |
Hello, I did not try it out, but I do not see a reason why the ASi Master would reply differently for given datasets depending on type of Interface of the IM of the ET200SP. My only comments here are that the ASi Master must have at least firmware V1.1. And that the reaction time could be slower on Profbus. |
Last edited by: jklm at: 4/1/2017 10:48:46 AMLast edited by: jklm at: 4/1/2017 10:49:18 AMBest regards |
|
Follow us on