10/20/2011 1:10 PM | |
Joined: 3/21/2006 Last visit: 9/10/2024 Posts: 10228 Rating: (1181)
|
AIO - http://support.automation.siemens.com/WW/view/en/37627 |
10/20/2011 3:58 PM | |
Posts: 60 Rating: (1) |
Ok, thanks for the feedback so, it is possible to install profibus network upto 500m without repeater |
10/20/2011 4:55 PM | |
Joined: 4/30/2007 Last visit: 3/9/2023 Posts: 231 Rating: (23) |
Yes you can, but I wouldn’t. Long distances are always a concern, signal attenuation, grounding issues and so on.Using a repeater only brings benefits, like but not limited to electrical isolation and signal strengthening. My recommendation is to use it, and I believe most of here agree the same. Regards, Marciano |
10/24/2011 12:33 PM | |
Posts: 60 Rating: (1) |
Marciano, thank for the advice I think, it is recommended to use repeater. How many repeater do you think that i suppose to use? |
6/9/2015 1:34 PM | |
Joined: 9/3/2014 Last visit: 3/13/2019 Posts: 4767 Rating: (123) |
|
Follow us on