1/10/2012 8:00 AM | |
Joined: 3/21/2006 Last visit: 4/25/2024 Posts: 10228 Rating: (1181) |
How do you specify the runtime for a timer via an operator panel, or how do you output the remaining runtime? |
1/10/2012 7:28 PM | |
Posts: 14 Rating: (0) |
I'm not entering time from operating panel. I just want to display the time which is read in my PLC ,on HMI as show in attached variable table. |
1/11/2012 4:30 PM | |
Posts: 3037 Rating: (192)
|
Hello Ranjan Kamath, You can see the displaying the time of PLC in the following FAQ. See the point 1. Transfer of the CPU system time to the operator panel How do you synchronize the date and time between an operator panel and an S7-300/S7-400 controller with WinCC flexible? Tweety |
1/11/2012 7:16 PM | |
Posts: 14 Rating: (0) |
Dear Tweety, I dont want to display PLC time on HMI. As my attachment shows i want to display that DB value which is "Time", on HMI. Plz do the needful. |
1/17/2012 1:46 PM | |
Posts: 14 Rating: (0) |
Dear Tweety, I need it to display direclty. In H:M:S format of just H: M is also fine.. Plz help |