9/2/2023 4:57 AM | |
Joined: 12/18/2014 Last visit: 9/17/2024 Posts: 33780 Rating: (4194)
|
Since you didn't write which LOGO you have exactly, I can only assume that you have the current LOGO! 8.3. In principle, you want a user to explain the manual and/or the online help to you in 3 sentences. You can't expect that, it took others years to understand the LOGO! and its programming. Especially since new functions have been added over the years. The LOGO! is designed for 16-bit integers and bit processing. Rough distinction: I can only recommend that you look at the following Siemens websites: Easy Entry in LOGO! and SIMATIC S7-1200LOGO!-Library – Simple application examplesLOGO!-Library – Functions for analog value processing and communicationLOGO!-Library – Simple and extended functions in LOGO! switching programLOGO! Simply ingenious. Simply more. Tips and tricks (Video)LOGO! Web Based Trainings |
Follow us on