4/1/2016 2:43 PM | |
Joined: 3/14/2008 Last visit: 7/2/2024 Posts: 2075 Rating: (930) |
Hi Mark, The "OS additional text" is generated when the attribute: "BLK_Jump" is generated for the variable. When the OS is compiled, an OS internal variable is created: "<blockname>.<variablename>#Jump". If the parameter is interconnected (ANY type), a text reference with the entry of the OS tagname of the interconnected block is created. |
Last edited by: Oreca at: 4/1/2016 2:43:56 PMIf I could help you, you can use the RATE button. Thank you. |
|
Follow us on