3/13/2020 2:55 AM | |
Joined: 7/5/2013 Last visit: 11/5/2024 Posts: 3118 Rating: (514) |
Hello K_Ohjus,
just a hint, there is already an example for showing the Audit Trail on a panel: WinCC Audit Trail Filter (filtering the operator actions on the SIMATIC Panel) Relating the checksum calculation, it's a Siemens secret in order to prevent one modifies the file and also cheats the corresponding checksum which would make the recording non-compliant. On the WinCC-DVD there is, besides the Audit Viewer, a tool to proof the checksum. But I never used that on a panel, only on a PC. Regards, Frink |
Pi is exactly three! |
|
This contribution was helpful to1 thankful Users |
Follow us on