5/28/2014 6:32 PM | |
Joined: 8/16/2010 Last visit: 11/5/2024 Posts: 638 Rating: (12) |
No, I dnot want complete solution. I just want to see how is the better to use signal from sensors in this situation? because of that I need information from experienced colegues. I have idea to use "address positive edge detection" like in attached example. AttachmentFC5.pdf (166 Downloads) |
5/28/2014 6:58 PM | |
Posts: 378 Rating: (73) |
Hello Milosh, As I have seen your process picture, it is a press machine which needs high personnal saftey and it may result serious injury. For example on your program you are not implemented Emergency switch, and also for closing the plates you may need to add two hand operation to make sure operator's hand are outside pressing area. Regards, |
This contribution was helpful to1 thankful Users |
5/28/2014 7:57 PM | |
Joined: 9/7/2007 Last visit: 10/9/2024 Posts: 550 Rating: (62) |
HiMilosh Have you read our experthuggy_d1in the thread:
|
Last edited by: Khaled_Ezzat at: 5/29/2014 9:12 AMBest Regards |
|
This contribution was helpful to1 thankful Users |
Follow us on