7/19/2020 5:55 PM | |
Posts: 19 Rating: (0) |
Hello all, I have been wondering if there is a way to join to open contacts and separate them according to convenience. The desired behaviour is join two open contacts, and this open contacts will start automatically an external generator, when it is enough, the two contacts will separate and the generator will stop. How this can be done? With two inputs? Please, find extra information attached. Any help is appreciate. Thank you in advance. Attachmentextra info.zip (254 Downloads) |
Last edited by: abe708 at: 07/19/2020 17:56:27 |
|
7/19/2020 6:21 PM | |
Joined: 12/18/2014 Last visit: 9/30/2024 Posts: 33855 Rating: (4210)
|
To do this, you would first have to know when and under certain circumstances you want to start the Genartor. |
7/19/2020 6:32 PM | |
Joined: 12/18/2014 Last visit: 9/30/2024 Posts: 33855 Rating: (4210)
|
I don't know your program. Which certain mark do you mean? You only have to use one LOGO! output.
|
7/19/2020 6:45 PM | |
Posts: 19 Rating: (0) |
Understood, I will use other mark with no special conditions. On the other hand, how can I use the relay output? Thank you. |
Follow us on