9/18/2023 10:48 AM | |
Joined: 11/28/2022 Last visit: 9/3/2024 Posts: 23 Rating:
|
Hello, I use MTP 1200 and MTP 1500. The resolution is different the ratio too... I use a method to autoscale MTP 1500 on a MTP1200 base project : => This is more or less what is descibed in this topic : Link to the topic My problem is that the ratio is different : It means that I have a "gray banner not beautifull" I don't know if somebody has a similar issue. I don't want to parameter the size of all objects of my project in function to the ratio. Edit : Could I have a solution to adapt a screen with size 100x100 on the parent WindowsSceen with a size 120/100? Thanks in advance. Regards, Manuel |
Last edited by: AutoGen_7017258 at: 09/18/2023 10:51:41 |
|
Follow us on