5/4/2022 10:33 AM | |
Joined: 11/6/2021 Last visit: 1/16/2023 Posts: 15 Rating: (0) |
Hi Georg, is it possible to activate autostart and graphics runtime in service mode and add to startup list? I have adopted a project in which autostart can't run even after latest 7.5 sp2 update 8. It says "autostart not possible" and I've tried everything regarding user control groups etc. The autostart log says that password or user is wrong or not in SIMATIC HMI group, but that's true, everything regarding service user is correct. I've also tried to add to the startup list in Communication Settings and it still doesn't work. ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 05/04/2022 12:56:58New subject after splitting. |
|
5/4/2022 12:56 PM | |
Joined: 6/19/2017 Last visit: 9/6/2024 Posts: 8175 Rating: (172) |
Closed cause question posted twice. The second thread with the subject Autostart is just not working properly in ServiceMode is published within the conference SIMATIC WinCC. Jen_Moderator |
Follow us on