9/9/2022 1:36 PM | |
Joined: 5/24/2022 Last visit: 1/8/2024 Posts: 16 Rating: (0) |
But it is running on server than I start it on client and shows this information |
9/12/2022 6:49 PM | |
Joined: 5/24/2022 Last visit: 1/8/2024 Posts: 16 Rating: (0) |
In Siemens manual to set autostart there is no NCGM section? Can you explain me what is this? |
9/14/2022 12:29 PM | |
Joined: 8/3/2009 Last visit: 4/26/2024 Posts: 12869 Rating: (1641)
|
Hello grzemuc does it work without autostart? -> Open Simatic Shell on the client and then richtclick on the project on the Server and connect from the client. does this work? If not then you should check the basics: https://support.industry.siemens.com/cs/de/en/view/108464289 ByeMurof |
If this Information really helps, you could use the Rate function |
|
Follow us on