1/10/2021 12:56 PM | |
Joined: 12/3/2018 Last visit: 1/22/2024 Posts: 76 Rating: (0) |
The vaules in praxis are 200 to 550 integer. |
1/10/2021 4:50 PM | |
Joined: 2/22/2008 Last visit: 5/8/2024 Posts: 2698 Rating: (206) |
See attachment for a possible solution and try to understand this principle, there are some comments at the blocks. It is also possible, that any mistake is in the program. After first start the average may be wrong, because the counter for amount is 0 at the beginning. Perhaps the program has to be expand for some options like reset or manual correction. This will be the next step, after you have checked this version. The timer is adjusted in B002, the sum of TH and TL is your intervall. For simulation you can change TL=0:90s for seconds. The sum in arithmetic block will be checked for a value greater than 9999, then 10000 are subtracted and the value counter will be increased. For the last arithmetic block, both counters must not exceed 32767, therefore this version only can be used for a "small" time period. 32767 / 24h / 60min = 22,7 days for the amount counter. The value counter has no overflow in this period with your max. value of 550. Maybe there are other versions possible with longer time periods, but this you can get from me now. Regards, Scorp AttachmentAverage2.zip (143 Downloads) |
1/11/2021 9:27 AM | |
Joined: 12/3/2018 Last visit: 1/22/2024 Posts: 76 Rating: (0) |
OK, got it. The working time is normally around 17-20 hours per day, so maybe I will reach a whole month. |