10/7/2022 11:41 PM | |
Joined: 2/26/2019 Last visit: 8/1/2024 Posts: 57 Rating: (0) |
I am new to Aws and LWE, and I also get an LWE download error. When I create the environment in AWS I can down load from LWE, but I get a 502 Bad Gateway error when i go to tge url. When I try to down load from LWE I can't. I get an error saying" No solution stack named '64bit Amazon Linux 2016.09 v2 running Tomcat 8.5 Java found.... I'm using Python on my PC, which is supported in AWS Beanstalk. Is Python supported in LWE or do I need to use Tomcat? Thank you ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 10/10/2022 04:13:00New subject after splitting |
|
10/16/2022 10:15 AM | |
Joined: 2/26/2019 Last visit: 8/1/2024 Posts: 57 Rating: (0) |
Please help. I have every solution offered in the forum and I cannot load my LWE application to AWS. I cannot create an environment from LWE. I keep getting the error listed in my first post. My LOGO is communicating. I've tried the workaround offered in the forum and when I down load I get the same error. Im attaching the LWE application zip as well. Please help, after 3 weeks of trying I'm at wits end as to how to get this working. Thank you, Dennis AttachmentSystem control.zip (623 Downloads) |
10/27/2022 12:46 AM | |
Joined: 12/18/2014 Last visit: 8/12/2024 Posts: 33542 Rating: (4166)
|
Start a Support Request. |
10/31/2022 11:38 AM | |
Joined: 2/26/2019 Last visit: 8/1/2024 Posts: 57 Rating: (0) |
Last post was meant for Philo. |
Follow us on