6/9/2010 5:29 PM | |
Joined: 3/21/2006 Last visit: 3/17/2025 Posts: 10239 Rating:
|
Hello, You need Seriell RS232 (6ES7 901-1BF00-0XA0) type of cable. Backup of project is possible to be done with either WinCC Flex, either with Protool software. Depends from which software was used there. In both cases upload is possible only if the project has been transfered to the panel with "Enable backtransfer" in wincc flex and "Enable upload". in Protool. The other easier way to do baskup/ restore of the project in TP170B is using Prosave software. (in case of used Protool it's version shopuld be at least 6.0). Look at How do you backup/restore with a Windows-based panel? Best regards, Hristo Mihalev |
6/10/2010 8:34 AM | |
Posts: 2 Rating:
|
thanks a lot!! Hristo Mihalev |
This contribution was helpful to
1 thankful Users |
Follow us on