Industry Online Support
Technical Forum
10/27/2006 1:51 PM | |
Joined: 4/24/2006 Last visit: 7/12/2024 Posts: 8711 Rating:
|
Hello, Do you know with wich software the OP15 is programmed, is it Protool or Comtext? Have you seen following link: http://support.automation.siemens.com/WW/view/en/21907703 I know with a OP17 you can put it in Transfer mode without deleting the project. There are two options: - The System screens are used in project, you can change mode by pushing button. - Or you can hold the buttons 'ESC and Cursor UP' when power comes on. Perhaps this also functions with OP15. Best regards, Wizard |
Last edited by: Wizard at: 10/27/2006 1:54 PM |
|
Follow us on