Industry Online Support
Technical Forum
3/31/2008 7:36 PM | |
Posts: 2 Rating: (0) |
Hi, I'm programming an interface between a Barcode Scanner and a PLC S7-300 (with S7 version 5.4). The program I am attaching is already working fine, with just one detail: it only gives me 16 characters and I need at least 20! If anyone could tell me what to do to have the next 4 characters I would appreciate it a lot!! Best Regards, Eduardo Peart AttachmentError_Pr.zip (509 Downloads) |
This contribution was helpful to1 thankful Users |
4/1/2008 4:59 PM | |
Posts: 2 Rating: (0) |
Hi Sydney, Thanks for your advise, I changed the RD1 to 20 bytes, but still can't see past the 16th character. I've also tried (FB1/Nw21&22) changing the LEN. Here's the program with the Neutral Lenguage check box selected... Regards, Eduardo Peart AttachmentError_C1.zip (374 Downloads) |
Follow us on