3/6/2014 7:34 AM | |
Posts: 36 Rating: (0) |
Need to re-build the tag logging again in the wincc server first?? |
7/24/2015 1:43 PM | |
Posts: 4 Rating: (0) |
Hello I have the same problem but I deal with WinCC without sever only . How can I fix the problem of Bdata archives I have the same log file of kernel Attachment201507241230092000.docx (422 Downloads) |
7/24/2015 1:49 PM | |
Posts: 4 Rating: (0) |
Hello I have a porblem with badata connection to wincc . You find here the attached of kernel trace . I checked the adress of data point, tag logging is running and the archives are available, Bdata kernel and WinCC are runnig under the same OS. But I still have the same error with all archives. Pleaaase help me Attachment201507241230092000.docx (418 Downloads) |
7/24/2015 2:02 PM | |
Joined: 1/27/2014 Last visit: 9/16/2024 Posts: 7 Rating: (1) |
Hi, Error "...line 809 ..." means that the datapoint is not available in WinCC. BR
|
Follow us on