4/9/2012 5:51 AM | |
Joined: 5/30/2008 Last visit: 10/11/2023 Posts: 135 Rating: (3) |
Dear experts, I am facing a problem which is desribed below. Please help me in resolving the problem. I am attaching herewith a project containing two stations - one is of CPU314-2DP and other is of CPU315-2DP. 1. In the staion of CPU315-2dp has one IM153-2 of order no. 6es7 153-2aa02-0xb0 along with other dp slaves of sinamics s120 CU320. 2. Under this DP slave (IM153-2DP) there are 2 DI, 1 DO, 1 AI and 1 AO modules. The AI and AO are actually only in hardware configuration. They ware not used in the programming. The project has been running very smoothly for last one year. 3. As the AI and AO modules are only in the hardware configuration and not used in the programming, I wanted to use these modules in other project. And because of this, I deleted the modules from the hardware configuration and recompile the configuration without any problem. Then downloaded the configuration to the stataion it belongs to. 4. After downloading the configuration, BF and SF leds for the CPU and IM153-2 are on. PLC is in run mode. In the diagnosois buffer, it is showning (though I can not not exactly remember at this moment), CPU can not detect the exact IM153-2 which has been in the hardware configuration. I will be highly grateful if anybody kindly help me in identifying the problem. Best regards, Shyamal AttachmentOnly-har.zip (189 Downloads) |
Follow us on