10/19/2020 2:52 PM | |
Posts: 5 Rating: (0) |
I'm experiencing a problem with a cnc machine with the following Sinumerik parts: Ascom Energy System 77-964-2300 Converter Operator Panel 6FC5203-0AB20-1AA0 MMC 6FC5210-0DA20-2AA1 PCI-ISA Box 6FC5247-0AA02-1AA0OP032S Keyboard 6FC5203-0AD10-1AA0 Full CNC Keyboard 6FC5203-0AC00-1AA0 Picture link: [snip] When start up the cnc machine the Operator Panel is Black or Blank, at the same time the Full CNC Keyboard and OP032S Keyboard's green LED flashes, after 10 minutes the Operator Panel screen went normal until I press the "input" key and all went back to black screen, Is it the wiring or the Ascom Power Unit should I be concerned? Please advise, Thanks, Freddy AttachmentPictures.zip (288 Downloads) |
Last edited by: Jen_Moderator at: 10/20/2020 08:06:16Removed link and added files as an attachment. Last edited by: a64664137 at: 10/20/2020 12:28:54Last edited by: a64664137 at: 10/20/2020 12:34:08 |
|
10/20/2020 12:23 PM | |
Posts: 5 Rating: (0) |
Hi Pee, The display on the main unit (MMC 103) is 0. I tried connecting an external display but nothing showed up. Swapped the Operator Panel and Ascom Unit, still no display... Have a look at this video: open attachment. Attachmenttrim.B8AF0DD7-C8E9-4456-8EAD-A202503369FF.MOV (278 Downloads) |
Last edited by: a64664137 at: 10/20/2020 12:26:25Last edited by: a64664137 at: 10/20/2020 12:33:10 |
|
10/20/2020 6:04 PM | |
Joined: 1/19/2008 Last visit: 10/2/2024 Posts: 992 Rating: (64) |
HI, The main unit is the 840D control system in the cabinet. Not the mmc which is just the front end. Pee |
10/25/2020 1:35 AM | |
Posts: 5 Rating: (0) |
Ok. There was a a red light on this unit: open attachment. |
11/18/2020 3:24 PM | |
Posts: 5 Rating: (0) |
Attachmentpictures2.zip (179 Downloads) |
Follow us on