Industry Online Support
Technical Forum
4/2/2008 6:21 PM | |
Posts: 2661 Rating: (279) |
Will the following links help? Programmable Controller S5-110A Timer/Counter module http://support.automation.siemens.com/WW/view/en/21190400 Upgrading from controllers S5-110A and S5-130A/K to controllers S5-115U and S5-135U http://support.automation.siemens.com/WW/view/en/2205332 The last time I used these modules was way back in the late eighties! Even then these were considered outdated!! I vaguely remember doing the time settings on the module. Probably it is easier for you to substitute timers in your S7 program after "understanding" the 110A program. All the best. |
4/2/2008 10:45 PM | |
Posts: 3 Rating: (0) |
Thats great, thank you. I did have a look in that area of product support but missed the "archived" folder! Thanks again. Roy |
5/1/2008 3:05 PM | |
Joined: 9/20/2006 Last visit: 3/5/2024 Posts: 307 Rating: (96) |
It is really surprising to see the s5 110 a systems being used even today. I was repairing these modules in the 1990's. |
Follow us on