2/24/2016 11:38 AM | |
Posts: 61 Rating: (11) |
It has been a while since I did anything S5, but ZYK is a cycle time error. I guess the normal cycle time of the PLC is very close to the limit, and the extra load caused by monitoring pushed it over the edge. You could add a call to OB31 in the middle of the program temporarily as described in this manual: https://support.industry.siemens.com/cs/attachments/1091648/6ES5_998-8MA22.pdf (page 9-6) to re-trigger the monitoring. There may be other methods, but this is the only one I could find with a quick google.
Brian |
Last edited by: Min_Moderator at: 2/24/2016 3:23:10 PMReplace link with permanent one |
|
Follow us on