2/12/2024 7:28 PM | |
Joined: 4/14/2022 Last visit: 10/14/2024 Posts: 5 Rating: (0) |
Dear All, I want your support to fix this problem. I am using Tia porta V16.0. cpu 1212 DC with CP card 1241(RS 232) Using "modbus_com_load"_and "modbus_master" i have established the communication but as per provided input register of slave device for voltage input register is 29792(5 digits) however in simulator it read on 329792(6 digits). as per modbus master block it show the range of input register 30001 to 39999(5 digits). any other block which support 6 digits input registers? any solution to solve this issue? or any conversion between 6 digits to make 5 digits input register or vice versa? Kindly find the attachment Thanks ------------------------------------------------------------------------------------------ |
Last edited by: The Helping Hand at: 02/14/2024 10:21:02New subject after splitting "through patience, great thing are accomplish" |
|
Follow us on