4/29/2013 10:09 PM | |
Joined: 10/29/2012 Last visit: 3/4/2024 Posts: 102 Rating: (1) |
I thought so. Thank you for your reply. |
6/24/2013 7:17 PM | |
Joined: 7/8/2009 Last visit: 7/26/2023 Posts: 1974 Rating: (477)
|
Ok so i guess there was a little confusion Now to orignal question - Dear Ugljesa Yes, you can set output current on Display. For that, you need to set 27 in P005. P005 is the Parameter for source of display in BOP For more about this and other Parameters, kindly refer Parameter List And also, for more about Micromaster, please refer to Operating Instruction - its a very nice manual and you will get very good details from this Regards, Devesh Vithani |
I dont Like people driving Fast, thats the reason I overtake them ;) |
|
This contribution was helpful to1 thankful Users |
Follow us on