Industry Online Support
Technical Forum
3/9/2021 10:36 AM | |
Posts: 1 Rating:
|
I have a few concern regarding our Engineering PC, I tried to connect the PC to the spare Lan cable and open the Runtime but after opening I observe no data from the was displayed. Graphics was fine but no reading from all transmitter. I did try to check some configuration using the Simatic Communication setting and observe that Simatic shell adapter Selection is on Terminal Bus[P1], while PlantBus [P2} is unselected. On the runtime error logs during opening is Connection error to device OS, Connection error to device AS, Configured Device name for the time synchronization.. With this I check the Full Computer Name and confirm it was correct. I did also check the IP address for [P1] and [P2] I did confirm there was no changes on the IP configuration. I also check the winCC program and when I open the time synchronization It has an error with Synchronization Via System Bus was uncheck or unselected. Is it normal? Both access point 1 and access point 2 have no value during this time. We have 2 OS and 1 ES/OS (engineering service laptop) ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 03/09/2021 13:19:32New subject after splitting |
|
Follow us on