Industry Online Support
Technical Forum
1/7/2014 8:36 AM | |
Joined: 4/22/2010 Last visit: 5/3/2024 Posts: 5697 Rating: (715)
|
Hello, you can not transfer a program to a card with a Logo without display. You have to use a type with display to program the card and then load the program in the pure logo See this older manual. There are some restrictions in what Logo you can use with the card. Which LOGO! memory/battery cards can be used with which LOGO! device series? Regards, Marcjan |
Last edited by: Marcjan at: 1/7/2014 8:42 AMProblem solved? |
|
Follow us on