3/1/2019 6:35 AM | |
Posts: 3 Rating: (0) |
I try to build iot2000 linux_x64 sdk to cross compile iot2000 program in x64 system(Ubuntu PC), I follow the steps in https://github.com/siemens/meta-iot2000. After several hours building, I get an error about node-red. Could anyone help to find the reason and how to solve? following is the detail output. ~/iot2040$ kas build meta-iot2000/meta-iot2000-example/kas-sdk-linux-x64.yml 2019-03-01 11:56:54 - INFO - kas 0.20.1 started 2019-03-01 11:56:54 - INFO - /home/gtf/iot2040/meta-iot2000/meta-iot2000-example$ git rev-parse --show-toplevel 2019-03-01 11:56:54 - INFO - /home/gtf/iot2040/meta-iot2000/meta-iot2000-example$ git rev-parse --show-toplevel 2019-03-01 11:56:54 - INFO - Using /home/gtf/iot2040/meta-iot2000 as root for repository meta-openembedded 2019-03-01 11:56:54 - INFO - /home/gtf/iot2040/meta-iot2000/meta-iot2000-example$ git rev-parse --show-toplevel 2019-03-01 11:56:54 - INFO - Using /home/gtf/iot2040/meta-iot2000 as root for repository meta-iot2000 2019-03-01 11:56:54 - INFO - /home/gtf/iot2040/meta-iot2000/meta-iot2000-example$ git rev-parse --show-toplevel 2019-03-01 11:56:54 - INFO - Using /home/gtf/iot2040/meta-iot2000 as root for repository meta-openembedded 2019-03-01 11:56:54 - INFO - /home/gtf/iot2040/meta-iot2000/meta-iot2000-example$ git rev-parse --show-toplevel 2019-03-01 11:56:54 - INFO - Using /home/gtf/iot2040/meta-iot2000 as root for repository meta-iot2000 2019-03-01 11:56:54 - INFO - /home/gtf/iot2040/meta-iot2000/meta-iot2000-example$ git rev-parse --show-toplevel 2019-03-01 11:56:54 - INFO - Using /home/gtf/iot2040/meta-iot2000 as root for repository meta-iot2000 2019-03-01 11:56:54 - INFO - /home/gtf/iot2040/meta-nodejs$ git cat-file -t 7e90d506488036cf1c490d1ac1086675eb2805b6 2019-03-01 11:56:54 - INFO - /home/gtf/iot2040/meta-openembedded$ git cat-file -t eae996301d9c097bcbeb8046f08041dc82bb62f8 2019-03-01 11:56:54 - INFO - /home/gtf/iot2040/meta-intel$ git cat-file -t 4ee8ff5ebe0657bd376d7a79703a21ec070ee779 2019-03-01 11:56:54 - INFO - /home/gtf/iot2040/poky$ git cat-file -t 2731fd35d5570263bc004ab16acf4acb0d94422b 2019-03-01 11:56:54 - INFO - Repository meta-nodejs already contains 7e90d506488036cf1c490d1ac1086675eb2805b6 as commit 2019-03-01 11:56:54 - INFO - Repository meta-openembedded already contains eae996301d9c097bcbeb8046f08041dc82bb62f8 as commit 2019-03-01 11:56:54 - INFO - Repository meta-intel already contains 4ee8ff5ebe0657bd376d7a79703a21ec070ee779 as commit 2019-03-01 11:56:54 - INFO - Repository poky already contains 2731fd35d5570263bc004ab16acf4acb0d94422b as commit 2019-03-01 11:56:54 - INFO - /home/gtf/iot2040/meta-iot2000/meta-iot2000-example$ git rev-parse --show-toplevel 2019-03-01 11:56:54 - INFO - Using /home/gtf/iot2040/meta-iot2000 as root for repository meta-iot2000 2019-03-01 11:56:54 - INFO - /home/gtf/iot2040/meta-nodejs$ git status -s 2019-03-01 11:56:54 - INFO - /home/gtf/iot2040/meta-nodejs$ git rev-parse --verify HEAD 2019-03-01 11:56:54 - INFO - 7e90d506488036cf1c490d1ac1086675eb2805b6 2019-03-01 11:56:54 - INFO - Repo meta-nodejs has already been checked out with correct refspec. Nothing to do. 2019-03-01 11:56:54 - INFO - /home/gtf/iot2040/meta-openembedded$ git status -s 2019-03-01 11:56:54 - INFO - /home/gtf/iot2040/meta-openembedded$ git rev-parse --verify HEAD 2019-03-01 11:56:54 - INFO - eae996301d9c097bcbeb8046f08041dc82bb62f8 2019-03-01 11:56:54 - INFO - Repo meta-openembedded has already been checked out with correct refspec. Nothing to do. 2019-03-01 11:56:54 - INFO - /home/gtf/iot2040/meta-intel$ git status -s 2019-03-01 11:56:54 - INFO - /home/gtf/iot2040/meta-intel$ git rev-parse --verify HEAD 2019-03-01 11:56:54 - INFO - 4ee8ff5ebe0657bd376d7a79703a21ec070ee779 2019-03-01 11:56:54 - INFO - Repo meta-intel has already been checked out with correct refspec. Nothing to do. 2019-03-01 11:56:54 - INFO - /home/gtf/iot2040/poky$ git status -s 2019-03-01 11:56:54 - INFO - D meta/recipes-extended/ghostscript/ghostscript/i586/objarch.h 2019-03-01 11:56:54 - INFO - D meta/recipes-extended/ghostscript/ghostscript/i686 2019-03-01 11:56:54 - WARNING - Repo poky is dirty - no checkout 2019-03-01 11:56:54 - INFO - /home/gtf/iot2040/meta-iot2000/meta-iot2000-example$ git rev-parse --show-toplevel 2019-03-01 11:56:54 - INFO - Using /home/gtf/iot2040/meta-iot2000 as root for repository meta-iot2000 2019-03-01 11:56:54 - INFO - /home/gtf/iot2040/poky$ /tmp/tmppd59um_4 /home/gtf/iot2040/build 2019-03-01 11:56:55 - INFO - /home/gtf/iot2040/meta-iot2000/meta-iot2000-example$ git rev-parse --show-toplevel 2019-03-01 11:56:55 - INFO - Using /home/gtf/iot2040/meta-iot2000 as root for repository meta-iot2000 2019-03-01 11:56:55 - INFO - /home/gtf/iot2040/meta-iot2000/meta-iot2000-example$ git rev-parse --show-toplevel 2019-03-01 11:56:55 - INFO - Using /home/gtf/iot2040/meta-iot2000 as root for repository meta-iot2000 2019-03-01 11:56:55 - INFO - /home/gtf/iot2040/build$ /home/gtf/iot2040/poky/bitbake/bin/bitbake -k -c populate_sdk iot2000-example-image Loading cache: 100% |#################################################################################################################################################################| Time: 0:00:00 Loaded 2791 entries from dependency cache. NOTE: Resolving any missing task queue dependencies Build Configuration: BB_VERSION = "1.36.0" BUILD_SYS = "x86_64-linux" NATIVELSBSTRING = "universal" TARGET_SYS = "i586-poky-linux" MACHINE = "iot2000" DISTRO = "poky-iot2000" DISTRO_VERSION = "2.4.3" TUNE_FEATURES = "m32 i586-nlp" TARGET_FPU = "" meta-intel = "HEAD:4ee8ff5ebe0657bd376d7a79703a21ec070ee779" meta-iot2000-bsp meta-iot2000-example = "master:1276e31be5563f624544e7c7a9323b8dcda858d5" meta-nodejs = "HEAD:7e90d506488036cf1c490d1ac1086675eb2805b6" meta-networking meta-oe meta-python = "HEAD:eae996301d9c097bcbeb8046f08041dc82bb62f8" meta meta-poky meta-yocto-bsp = "HEAD:2731fd35d5570263bc004ab16acf4acb0d94422b" Initialising tasks: 100% |############################################################################################################################################################| Time: 0:00:05 NOTE: Executing SetScene Tasks NOTE: Executing RunQueue Tasks WARNING: node-red-0.16.2-r0 do_fetch: Failed to fetch URL npm://registry.npmjs.org;name=node-red;version=0.16.2, attempting MIRRORS if available ERROR: node-red-0.16.2-r0 do_fetch: Fetcher failure: Fetch command export PSEUDO_DISABLED=1; export SSH_AUTH_SOCK="/run/user/1000/keyring/ssh"; export PATH="/home/gtf/iot2040/build/tmp/sysroots-uninative/x86_64-linux/usr/bin:/home/gtf/iot2040/poky/scripts:/home/gtf/iot2040/build/tmp/work/i586-nlp-32-poky-linux/node-red/0.16.2-r0/recipe-sysroot-native/usr/bin/i586-poky-linux:/home/gtf/iot2040/build/tmp/work/i586-nlp-32-poky-linux/node-red/0.16.2-r0/recipe-sysroot/usr/bin/crossscripts:/home/gtf/iot2040/build/tmp/work/i586-nlp-32-poky-linux/node-red/0.16.2-r0/recipe-sysroot-native/usr/sbin:/home/gtf/iot2040/build/tmp/work/i586-nlp-32-poky-linux/node-red/0.16.2-r0/recipe-sysroot-native/usr/bin:/home/gtf/iot2040/build/tmp/work/i586-nlp-32-poky-linux/node-red/0.16.2-r0/recipe-sysroot-native/sbin:/home/gtf/iot2040/build/tmp/work/i586-nlp-32-poky-linux/node-red/0.16.2-r0/recipe-sysroot-native/bin:/home/gtf/iot2040/poky/bitbake/bin:/home/gtf/iot2040/build/tmp/hosttools"; export HOME="/tmp/tmpajj6vef6"; /usr/bin/env wget -t 2 -T 30 -nv --passive-ftp --no-check-certificate --directory-prefix=npm/node-red https://registry.npmjs.org/to-absolute-glob/-/to-absolute-glob-2.0.1.tgz failed with exit code 4, output: Unable to establish SSL connection. ERROR: node-red-0.16.2-r0 do_fetch: Fetcher failure for URL: 'npm://registry.npmjs.org;name=node-red;version=0.16.2'. Unable to fetch URL from any source. ERROR: node-red-0.16.2-r0 do_fetch: Function failed: base_do_fetch ERROR: Logfile of failure stored in: /home/gtf/iot2040/build/tmp/work/i586-nlp-32-poky-linux/node-red/0.16.2-r0/temp/log.do_fetch.18612 ERROR: Task (/home/gtf/iot2040/meta-iot2000/meta-iot2000-example/recipes-node/node-red/node-red_0.16.2.bb:do_fetch) failed with exit code '1' NOTE: Tasks Summary: Attempted 4290 tasks of which 4289 didn't need to be rerun and 1 failed. Summary: 1 task failed: /home/gtf/iot2040/meta-iot2000/meta-iot2000-example/recipes-node/node-red/node-red_0.16.2.bb:do_fetch Summary: There was 1 WARNING message shown. Summary: There were 3 ERROR messages shown, returning a non-zero exit code. Error logfile is as attachment. Thanks! Attachmentlog.do_fetch.18612.txt (101 Downloads) |
Last edited by: gao1158 at: 3/1/2019 9:09:06 AM |
|
3/4/2019 3:32 AM | |
Posts: 3 Rating: (0) |
Dear jan-k, thanks for your reply. I do not use corporate network, and have not configure network. But in the end of the log file, It try to fetch from http://sources.openembedded.org/npm_node-red-0.16.2.tar.xz. I could reach http://sources.openembedded.org, but it does not have npm_node-red-0.16.2.tar.xz, so get 404 Not Found. I am not sure whether this is the point to failed. |
3/8/2019 8:31 AM | |
Posts: 3 Rating: (0) |
thanks for your reply! I will try it again. |