1/29/2014 10:37 AM | |
Posts: 1 Rating: (0) |
Hi, I face the same situation like Steven.So I dianostic to the master CPU in HW configuration.What I found is " Module configured but not avarible".Please see capture in atttached. So, My question are; Do I have to reconfigure bus module from 6ES7195-7HD00-0XA0 to 6ES7195-7HD10-0XA0 and re-download to the master CPU? If the answer is "YES".Please advice me how to re-configure 6ES7195-7HD10-0XA0 to compatible with the existing IM153-2 module(6ES7153-2AA02-0XB0) If the answer is "NO" then why does the problem still persists.I got comfirmed that IM153-2(6ES7153-2AA02-0XB0) are working. AttachmentBusmodule.zip (398 Downloads) |
1/29/2014 11:44 AM | |
Posts: 1368 Rating: (126) |
Hello, please notice that when the new bus module (6ES7195-7HD10-0XA0)is used, the new IM153-2 (6ES7153-2Bx00-0XB0) must be used as well. http://support.automation.siemens.com/WW/view/en/5670442 greetings, Pittiplatsch |
Last edited by: Pittiplatsch at: 1/29/2014 11:45 AM |
|
10/31/2015 5:13 AM | |
Posts: 2 Rating: (0) |
""Fault safety card channel are passivated, I don't know this mean. |
Last edited by: SeikKun at: 10/31/2015 5:14:55 AM |
|
7/21/2016 9:04 PM | |
Joined: 9/27/2006 Last visit: 4/27/2024 Posts: 12257 Rating: (2665) |
Reply provided by P.M. earlier: Hello; The following FAQ provides a basis for the diagnostic messages you are getting: yhe IM 153-2AA02 is not compatible with the active bus module BM 195-7HD10. Unfortunately, your choices seem to be to either upgrade the IM 153-2 (to a 153-2BA02, for example) or owngrade the BM 195 (to 195-7HD00, if it is possible to locate one). I dpo not think that a simple hardware configuration change will allow the modules to exchange data. Which bus modules can you use with the interface modules of the ET 200M? https://support.industry.siemens.com/cs/fr/en/view/109479504 Hope this helps, Daniel Chartier |
This contribution was helpful to1 thankful Users |
Follow us on