5/10/2013 10:32 AM | |
Posts: 48 Rating: (0) |
Where can I fint it in the program? |
5/15/2013 8:54 AM | |
Posts: 5225 Rating: (1187) |
Adam: A good idea you have there. There are many variations on the theme.. and you came up with one that I have not thought about. Emil: We all are assuming you wanting to make a toggle switch code. Do you mind if I weigh in on two variations? Please note the samples include coding to force a switch off on "first scan". Add to this whichever conditions you see fit. In the S7 PLC range the toggle action is not a standard function. In the Logo! there is a function handling this that is worth looking at. Let us know if that is what you wanted. PS: Note that the colour scheme in my software is not normal. The white background hurts my eyes. Greetings, w Attachmenttoggle.zip (44 Downloads) |
Follow us on