5/29/2011 8:15 PM | |
Posts: 22 Rating: (0) |
Is there any codes in C to write the time value from the WINCC runtime to the pc time. I seen a project with visual basic. what are the experciences? |
5/29/2011 8:25 PM | |
Joined: 3/21/2006 Last visit: 4/25/2024 Posts: 10228 Rating: (1181) |
Hello, Perhaps How can you read out, display or set the local computer time or the coordinated world time in WinCC Runtime? best regards, Hristo Mihalev |
5/30/2011 8:38 AM | |||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
Joined: 10/3/2010 Last visit: 4/29/2024 Posts: 1552 Rating: (188) |
Entry ID:24019500 Instructions: You can set or read the system time with the following functions:
A distinction is made in the system between the local computer time and Greenwich Mean Time. The "SetSystemTime / GetSystemTime" functions can be used to set or read Greenwich Mean Time. The following examples show how the local computer time is read or set in WinCC: Example:
Example:
Example:
Example:
The time-of-day parameters for setting the time can be specified via internal WinCC variables, e.g. via IO fields in the process image A simple vbs method: http://motevich.blogspot.com/2007/10/qtp-set-get-system-time-date.html |
||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
Last edited by: SteBo at: 5/30/2011 8:50 AMadded VBS Last edited by: SteBo at: 5/30/2011 8:39 AMB r g d s , |
|||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
5/30/2011 2:19 PM | |
Joined: 10/3/2010 Last visit: 4/29/2024 Posts: 1552 Rating: (188) |
to give you a clue, this should be possible: put/read PLC time in an internal/external tag of WinCC, put & adjust your script from the button in a global script triggered by an action (internal value = 12) |
Last edited by: SteBo at: 5/30/2011 2:24 PMB r g d s , |
|
5/30/2011 2:35 PM | |
Joined: 10/3/2010 Last visit: 4/29/2024 Posts: 1552 Rating: (188) |
varname can be for example an internal WORD tag in which you store PLC-time |
B r g d s , |
|
5/30/2011 2:49 PM | |
Posts: 2661 Rating: (279)
|
Hi SRV, I now understand what you need... I'll try for solution. Regards |
This contribution was helpful to1 thankful Users |
Follow us on