12/9/2015 11:17 AM | |
Joined: 4/24/2006 Last visit: 11/5/2024 Posts: 8766 Rating: (1170) |
Hello, The C7-635 is based on an TP/OP170B. Perhaps the following link might help: Which connector cables are available for connecting to SIMATIC Panels? An OS update with the option "Reset to factory settings" might be possible, if you use a Null-modem cable. Have a look here: how can you transfer a WinCC flexible project serially to a panel? And: Best regards, Wizard |
Follow us on