Industry Online Support
Technical Forum
8/7/2013 8:59 AM | |
Joined: 4/24/2006 Last visit: 11/5/2024 Posts: 8766 Rating: (1170)
|
Hello Nibsy, I've found the following link: how can you make a project backup from an operator panel? (But C7-636 is not mentioned ) Since C7-635 is based on CPU314 and OP270, you should use the following link: how do you backup/restore with a Windows-based panel? Best regards, Wizard |
8/7/2013 9:44 AM | |
Posts: 6 Rating: (0) |
Hi Wizard, Thanks for that. In work now and discovered I got the model number wrong it's actually a C7-626! |
8/7/2013 9:57 AM | |
Joined: 4/24/2006 Last visit: 11/5/2024 Posts: 8766 Rating: (1170)
|
Hello Nibsy, Oh, the C7-626 was based on OP25 Have a look at the following link: how do you back transfer the projects of an operator panel and what should you watch out for? have a look at "back_transfer_devices_e", then you will find out that with C7-626, uploading and Backup/restore is not possible Best regards, Wizard |
Follow us on