2/15/2011 8:21 PM | |
Posts: 259 Rating: (5) |
Hi, Thx for replay. I have one more question i make my own cable and it looks like that: Computer (RS232) 810T(LPT) 9Pin 25Pin Pin 2 Pin 2 Recive-Transmit Pin 3 Pin 3 Transmit-Recive Pin 4 Pin 6 DTR-DSR Pin 5 Pin 7 Ground-Ground Pin 6 Pin 20 DSR-DTR Pin 7 Pin 5 RTS-CTS Pin 8 Pin 4 CTS-RTS
I know that this cable works with Pcin and 810T. What you think it will be working with step5 and 810?
With regards, makaveli Splitted from How download PLC do PG with Step5?. |
Last edited by: O_Moderator at: 2/16/2011 8:22 AMnew subject after splitting |
|
2/16/2011 8:06 AM | |
Joined: 3/21/2006 Last visit: 4/25/2024 Posts: 10228 Rating: (1181)
|
Hello, Look there and compare it S5 programming cable Best regards, Hristo Mihalev |
2/16/2011 9:00 AM | |
Joined: 12/12/2005 Last visit: 3/17/2024 Posts: 180 Rating: (12) |
Hi, What is your 810 plc MLFB number of SIMATIC. I think better use original cable my 6ES5734-2BF00 cable is PG connection COM/TTY male 25pin and S5 PLC/AG side 15pin male. http://support.automation.siemens.com/WW/view/en/27610457 I think you are not need this cable, because you candownload program from panel not from PLC unit? -Heksu- |
Last edited by: Heksu at: 2/16/2011 9:47 AM"Beer is proof that God loves us and wants us to be Happy"-Benjamin Franklin |
|
2/25/2011 3:54 PM | |
Posts: 259 Rating: (5) |
Hi, I borrow cable for S5 AG/TTY (6ES5 734-1BD20). But still i have problem this cable is from one side men DB15 and from another female DB25. I have on machine-Sinumerik 810T female DB25 and in computer RS232 and also LPT port (I prefer RS232 DB9). So right now i need more conveners from Sinumerik 810T site i need to change female for men because it is not possible co connect female to female:-) And from computer side other cable to change DB15 to RS232(DB9). I will by great full for schema how to make connection in both cables. In attachment you can see my cables. With regards, makaveli AttachmentBorrowCable.zip (482 Downloads) |
2/28/2011 12:31 PM | |
Posts: 259 Rating: (5) |
Any advise... With regards, makaveli |
Follow us on