4/6/2016 6:21 PM | |
Joined: 6/3/2014 Last visit: 1/17/2023 Posts: 660 Rating: (192) |
Hello AndreasC, the example you chose is not exactly the easiest if you're new with faceplates. I would recommend the following application example:
It has a detailed documentation on how to create faceplates and an example project. Do you have a special interest in this particular faceplate or do you just want to dissect one to see how it works? |
~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ★ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ |
|
This contribution was helpful to1 thankful Users |
4/7/2016 10:37 AM | |
Posts: 14 Rating: (0) |
I am interested in using faceplates for motors and valves in a project. Mostly to save time and also to make the controls easier to read and so on... all the advantages of faceplates I guess I have no problem using the ones I got in the first link execept for when it comes to the comfort panel at the time. |
Follow us on