5/3/2016 7:34 PM | |
Posts: 1 Rating: (0) |
Dear Sir I want to callibrate my op177b touch screen as sometimes it is not working. Please tell me how to fix this problem. This is a test run vdo wrong . Thanks & Regards Aphirak Thailand |
Last edited by: maiati at: 5/3/2016 7:38:54 PM |
|
5/3/2016 8:14 PM | |
Joined: 3/28/2015 Last visit: 8/25/2024 Posts: 721 Rating: (213) |
Hello, 1-Do the HMI Calibration as in the attached file. 2-You can use an external USB mouse to avoid the breakdown time . 3-If the problem not solved, try to do OS update with option "reset to factory settings" Which connector cables are available for connecting to SIMATIC Panels? then download the program to the panel. AttachmentCalibrating the Touch Screen.pdf (166 Downloads) |
Eng.Mohamed Ibrahim |
|
Follow us on