1/12/2016 6:50 PM | |
Joined: 12/18/2014 Last visit: 5/27/2024 Posts: 33109 Rating: (4087) |
Now here is my proposal for a possible solution. The output of the AND block B042 corresponds to the output of the simulated "second weeks timers". AttachmentSimulation_of_second_weekly_timer.zip (219 Downloads) |
1/12/2016 10:44 PM | |
Joined: 12/27/2006 Last visit: 5/23/2024 Posts: 1196 Rating: (113) |
You can use the time of the clock (ON/OFF or Days) by using VM mapping. You must make a virtual point of it. But the times are in a kind of HEX format, so you must make a lot of cacqulations. I have make a little start with it. It only works good for times to 9.59 (9 Hour 59 minutes) becouse the HEX format make it not good after it. Look in the HELP of Logo soft comfort for Parameter VM Mapping. So this is only a start AttachmentKlokkenspel.zip (209 Downloads) |
1/12/2016 11:50 PM | |
Posts: 65 Rating: (1) |
Thanks for you help guys got some ideas on how to do it. |
1/13/2016 5:53 AM | |
Joined: 12/18/2014 Last visit: 5/27/2024 Posts: 33109 Rating: (4087) |
@Toeternietoe, your program doesn't work correctly. AttachmentUnbenannt.zip (212 Downloads) |
1/13/2016 9:58 PM | |
Joined: 12/18/2014 Last visit: 5/27/2024 Posts: 33109 Rating: (4087) |
That's why I've chosen a different path in my program. |
Follow us on