3/1/2024 5:24 PM | |
Joined: 3/24/2023 Last visit: 5/30/2024 Posts: 1 Rating: (0) |
Hello, I have an AS-I master gateway device, ASI V3. I have slave devices connected to it, all of the same make and model. The brand of my master and slave devices is the same. Is it possible to use another brand of slave module in this master module? (I can choose ASI V3 for the slave module to be compatible with my master module) Thank you very much for your feedback. TRANSLATE with x English TRANSLATE with Enable collaborative features and customize widget: Bing Webmaster Portal |
Last edited by: The Helping Hand at: 03/04/2024 10:52:32Text formatting optimized |
|
3/1/2024 9:15 PM | |
Joined: 9/15/2006 Last visit: 5/28/2024 Posts: 470 Rating: (80) |
For sure you can use ASi slaves from different brands. ASi is standardized. |
Follow us on