8/30/2024 6:00 AM | |
Joined: 12/18/2014 Last visit: 10/14/2024 Posts: 33956 Rating: (4221) |
You ask the same in this topic: Is it Possible to Transfer Audio file to TP700 Comfort |
8/30/2024 6:47 AM | |
Joined: 11/21/2020 Last visit: 10/14/2024 Posts: 175 Rating: (0) |
It is deleted. |
8/30/2024 2:35 PM | |
Joined: 7/7/2010 Last visit: 10/14/2024 Posts: 15302 Rating: (2427)
|
The manual and FAQ referenced in the linked post are all available. The FAQ describes the external program call to launch the preinstalled CE media player as well as suggests additional software which may help target media specifications of the TP700 Comfort - and other panels. You do of course need the Comfort Panel (or Advanced / Runtime Advanced) - for others searching and finding this forum post in the future.
|
science guy |
|
8/30/2024 4:56 PM | |
Joined: 11/21/2020 Last visit: 10/14/2024 Posts: 175 Rating: (0) |
Don't be sad, this one is dummier than two of us: |
Follow us on