11/29/2018 4:16 PM | |
Posts: 20 Rating: (3) |
Same problem here. I am using a S7-1500, which according to Siemens documentation uses "Little-endian". When a message received via TCP/IP is deserialized into (for instance) an array of REAL, the decoded REAL values from the output of Deserialize() are written with the assumption that the input stream is in big-endian order. Can Deseralize be configured to work little or big endian ? ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 11/30/2018 10:41:56 AMNew subject after splitting |
|
12/5/2018 2:45 PM | |
Posts: 20 Rating: (3) |
According to this link, the S7-1500 CPU architecture is little-endian... https://support.industry.siemens.com/tf/ww/en/postattachments/imagecontainer/?attachmentId=68415 |
12/5/2018 8:42 PM | |
Joined: 9/21/2012 Last visit: 5/23/2024 Posts: 3948 Rating: (446) |
That has been taken out of context... |
Last edited by: Hati at: 12/5/2018 11:25:40 PMTypos |
|
Follow us on