10/14/2019 1:36 PM | |
Joined: 6/4/2010 Last visit: 9/30/2024 Posts: 387 Rating: (130)
|
Dear forum member, You did not mention if you migrated from Desigo Insight or from Apogee Insight. Desigo CC is the successor of both “insights”. Anyway, the Desigo CC provides an SNMP client, but it does NOT provide a SNMP server functionality in the current version. Desigo CC has a build in OPC server to provide data to other systems. Therefore the recommendation is to use the build in OPC server feature to provided data to an other system. For further information please see documentation, Online Help. Best regards, Albis |
Follow us on