4/27/2020 2:09 PM | |
Posts: 36 Rating:
|
Hi! I have a question about this problem. I got a project what I need to modify (adding extra modes and etc.). It is in TIAP V11 so I upgraded to V13 SP1. For "home-testing" we made a testing area with a similar PLC. I did the change device command made the changes, tested it and would like to change the device back but the -AG31- isn't available in V13. I know about the hardware packages but those only changes hardware cataloge and I'd like to put my project to the old PLC by one click. Is there any solution to expand the opportunities in the changing device command? Thanks! ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 04/28/2020 08:10:53New subject after splitting |
|
Follow us on