4/8/2014 10:42 AM | |
Posts: 27 Rating: (14) |
When using string functions in Siemens the first two bytes must specify the maximum string length and the actual string length as in the attached example. For your application use FC38 String_I from the Standard Library / IEC Function Blocks instead of FC37 AttachmentAscii string handling.zip (299 Downloads) |
This contribution was helpful to2 thankful Users |