2/21/2008 11:06 AM | |
Posts: 5 Rating:
|
Hi all How i can stop my program or timers which are in my program and timers remember they current value? In this case i need stop program or timers if pause button (Input3) are pressed and if input 3 goes off, timers continues theirs current value. I attach example program.(Program is for monitoring. If I2 pulse doesent come in 24seconds, program give error and user must press Error acknowledgment button ) Thank you! Best Regards Joni Räsänen Finland ps. Sorry about my language, i am not very good speak English. Attachmentexample_joni_r.zip (962 Downloads) |
This contribution was helpful to
1 thankful Users |
2/21/2008 11:50 AM | |
Posts: 2930 Rating:
|
Hi, here is you programm modified: Changes: 1. Replaced your On-Delay by Retentive On-Delay and Retentivity enabled 2. Retentivity for your timer B002 enabled Please check if this modification is what you expect. Regards Helmut Attachmentexample_joni_r_V2.zip (1104 Downloads) |
2/21/2008 1:52 PM | |
Posts: 38 Rating:
|
Hi my friend, I hope this helps Best Regards from Argentine Kloopy Attachmentexample_joni_r.zip (931 Downloads) |
2/21/2008 2:36 PM | |
Posts: 5 Rating:
|
Hello First i thank you very much to help but maybe i need explain my system more. I think i am vainly confused you to my first example. Program monitoring system greasing. Sensor send pulse if grease go in system if pulse doesnt come in 24 hours(24secs in simulation) Logo gives error to service guy and he/she can check the system. If pause button are pressed, then grease dont go in system(another system control grease pumps) and sensor doesnt send pulse and i dont want make pointless errors to system users. That its my program idea. I cant restart timer in pause button because If timer value are 12 hours and i reset it, greasing spot maybe with out grease and warning comes at the earlist 24hours and its 12hours late :) Pause button is for service guy who need maintenance other system. I remove grease quantity for this example because its pointless in this "timer problem" :) So i want pause timer B001. I hope you understand my language, so i say before i dont speak english very well and write even worst. Regards Joni Räsänen Attachmentexample_joni_r.zip (742 Downloads) |
2/21/2008 9:28 PM | |
Posts: 191 Rating:
|
Hi!! try this.. hope this helps!! ROSA Attachmentexample_joni_r.zip (1448 Downloads) |
This contribution was helpful to
2 thankful Users |
4/29/2008 10:53 AM | |
Posts: 1 Rating:
|
Hi! I need this "pause-timer" aswell. But what do I do with this zip file?? Where do I put the file"example_joni_r.lsc". ??? Greetings... |
4/29/2008 5:04 PM | |
Posts: 191 Rating:
|
Hi!! try opening it with Logo! Soft comfort.. you can download thedemo version from http://support.automation.siemens.com/WW/llisapi.dll?func=cslib.csinfo&lang=en&siteid=cseus&aktprim=0&extranet=standard&viewreg=WW&objid=10805245&treeLang=en hope this helps!! ROSA |
4/29/2008 11:12 PM | |
Joined: 1/5/2007 Last visit: 4/7/2023 Posts: 1690 Rating:
|
Hi, for all with interrests - i have published in the german part a program for a bottle filling machine at /tf/WW/de/Posts/15961 In the attachment from my article at the 29.02.2008 i have programed 3 timers witch can start, stop, and clear. A sensor detect a bottle and starts one timer. If the time finish then the band stops and the bottle can filled. Between sensor and filling station can be 0 or 1 or 2 or 3 bottle and each one starts one timer and all timers stoped if a bottle comes under the filling point, after filling the band pover starts again and the timers are going too.. I thinkyou can find the 3 timers - Link to the attachment: DEMO_Bandabfuellung_V01.zip Best regards Betel |
==> Meine TAG-Listen: "deut." |
|
Follow us on