2/16/2014 6:53 AM | |
Joined: 4/14/2010 Last visit: 11/11/2024 Posts: 525 Rating: (11) |
Dear Siwarexi, Can i use attached load cell CZL 632 with 7MH4950-2AA01 module..?? One 7MH5103-3PD00 Load cell giving the 225mV on Sig+ Sig- when 150 kg load applied on it and module giving the SF fault i confirm the channel is ok but SIWATOOL display operational error ADC overload. Charactristic value configured 2mV this fault occure after 2 month it was working good. now we have no in stock the spare 7MH5103-3PD00 Can i use attached load cell CZL 632 with 7MH4950-2AA01 module..?? CZL632 load cell specifications:
Thanks AttachmentCZL-632 ,50-2500 Kg [ PARALLEL BEAM STYLE ].pdf (357 Downloads) |
Last edited by: GrasserF at: 2/19/2014 10:48 AMnew subject after splitting from /tf/WW/en/Posts/96577#top Last edited by: Sarfraz Bhatti at: 2/16/2014 3:06 PMMS |
|
2/19/2014 10:22 AM | |
Joined: 4/14/2010 Last visit: 11/11/2024 Posts: 525 Rating: (11) |
Thanks Siwarexi, We have installed One 7MH5103-3PD00 Share beam Loadcell on Rolloer Conveyor application is it suitable for this application. We are searching for route cause of load cell damaging i think if there will be electrically problem occure then also module channel will be faulty, but both channel are OK i have interchnged the another healthy load cell cable whats you opinion..?? Or any problem with mechanical structure design, please see attached installed location. actual load which is applied on it including conveyor weight = 450kg and load cell capacity is 500kg. CZL 632 is Parallel beam type capacity 2000kg, is it approperiate for this application..?? see attached. Thanks. Attachmentpic.zip (346 Downloads) |
Last edited by: Sarfraz Bhatti at: 2/19/2014 2:49 PMMS |
|
2/21/2014 1:52 PM | |
Joined: 4/14/2010 Last visit: 11/11/2024 Posts: 525 Rating: (11) |
Thanks for message, yes plate form is large size 1200x1200mm actually i am at not front of control panel but i can send you offline data please see attached. for Single load cell i have used manual weight adjustment according to mechanical structure behaviour. Auto Calculate adjustment digit was not possible result was tottally unexpected as 2mV/V Charachtristic value and offset in uV/V. Thanks. AttachmentLC_CH1-CH2.zip (330 Downloads) |
MS |
|
Follow us on